Introduction
Setup must be performed after the physical installation of the TeSys island and all other hardware devices and verification of the TeSys island topology. The following table summarizes the setup steps. The person performing the setup must be familiar with the TeSys island modules and avatars .
Setting up TeSys™ island
|
Step |
Action |
|---|---|
|
1 |
Power up the TeSys island . |
|
2 |
Connect to the TeSys island with the TeSys Island DTM or Operation and Maintenance Tool (OMT). |
|
3 |
Set the island IPv4 address, if connected via OMT. |
|
4 |
Import the project file to the TeSys Island DTM. |
|
5 |
Configure the TeSys island parameters. |
|
6 |
Connect to the TeSys island with SoMove software. |
|
7 |
Load the project file to the TeSys island . |
|
8 |
Verify the system installation in Test mode. |
|
9 |
Verify the TeSys island configuration. |
|
10 |
Verify the system wiring. |
|
11 |
Apply mains power. |
|
12 |
Use Force mode to simulate commands from the PLC. |