DOCA0270EN-02

Motor One Direction - SIL Stop, W. Cat 1/2

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

Wiring

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?