Fiber Cable Configurations

Some fiber objects have more options in the configuration that must be set for the data to work correctly. The FiberOpticCable object class has additional settings in the Fiber Object tab of Solution Center that further describe the type and strand count of fiber cables.

You can select cable attributes that are applicable for the Number of Strands, indicating Overhead or Underground, the Sheath Type, and whether the cable count quantity is Single Mode or Multi Mode.

Here is one example of how these menus are set.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.