Favorites Migration Best Practices

Fiber editors and designers rely on a pre-configured equipment catalog to efficiently build and maintain the GIS network. Fiber Manager supports fiber favorites for this purpose. While some Fiber Manager 10.x customers with small favorites catalogs can manually recreate their favorites in Fiber Manager XI, those with large favorites libraries need to migrate them from 10.x to XI.

In Fiber Manager10.x, favorites are stored in the geodatabase, whereas in Fiber Manager XI they are stored in a hosted repository. Also, the format of favorites storage changes in XI. Therefore, favorites migration requires you to export the favorites file from 10.x and then to change that XML file to the JSON format required by XI. Once changed, you can import the file to the XI repository.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.