Update the Autoupdater XI SOI Extension

Once you have deployed the Autoupdater XI SOI extension, follow these steps to update it:

  1. In ArcGIS Server Manager, click Site on the horizontal bar toward the top of the page.

  2. Click Extensions on the vertical bar near the left side of the page.

  3. In the list under Display Name, locate Autoupdater XI SOI, then click the Edit button under Action.

  4. In the dialog that opens, browse for the updated SE.Geospatial.Autoupdater.SOI_ent.soe extension file, select it, and click Save. Whenever you update the Autoupdater XI SOI extension, the process causes any feature service that was running it to stop.

  5. Open the Services app and restart all feature services that use the Autoupdater XI SOI extension.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.