Update the Fiber Manager SOE

Once you have deployed the Fiber Manager XI SOE extension, follow these steps to update it:

  1. From the horizontal bar at the top of the page, click Site.

  2. On the left hand side menu, click Extensions.

  3. In the list under Display Name, locate FiberXIRestSOE. Then under Action, click Edit.

  4. In the dialog that opens, browse for and select the updated FiberXIRestSOE_ent.soe file, then click Save. If desired, repeat the process for the ArcFM Autoupdater XI SOI.

    IMPORTANT: When you update the FiberXIRestSOE extension file, the update process stops any feature service running that extension.

    1. To view or change any SOE configuration parameters, follow the steps in the Configure the Fiber Manager SOE topic, scroll to the top of the window, and click Save.

    2. To view or change any SOI configuration parameters, follow the steps in the ArcFM Autoupdater XI SOI topic, scroll to the top of the window, and click Save.

  5. From the Services page, start all stopped services.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.