Circuit Bulk Healing

When you have copied the data, such as the name, header Globalid, Header class-model-name, and other optional information, for the migrated circuits to the new circuit table, the next step is to use the Circuit Bulk Healing tool functionality to identify and record the remaining fiber network facilities that must be associated with each circuit.  See the Circuit Bulk Healing tool topic for more information on how this tool finishes populating the migrated information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.