Check the Feature Layer Names

Before you start editing your data, you must make sure that the feature names listed in the published feature service, the Solution Center configuration, and the editing project layer names all match.

Here is an example with Device Point.

Device Point listed in the published feature service.

Device Point listed in the Solution Center configuration file.

Device Point listed in the ArcGIS Pro editing project.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.