EIO0000005724.00

Information

Displays the system status, version information, etc.

Function

Description

System Status

The system status and version information.

ETH1/ETH2

The network properties.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?