EIO0000005724.00

System Update

Updates the firmware and operating system of this product.

For instructions, refer to Update the System.

To perform this function, either an optional SD card or a commercially available USB storage device is required. Please prepare the external storage formatted with the FAT, FAT32, or exFAT file system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?