EIO0000005724.00

Using the Web Browser

This product displays the screen of a web server device on the intranet using a dedicated web browser.

This section describes how to use the dedicated browser for this product.

No.

Description

1

Displays the title of the web server page. If the page has no title, its URL is displayed instead.

While the browser is not in use, the title bar at the top of the screen is hidden.

2

Each time you touch Switch server icon, the displayed web server page changes.

3

Return to the previous page.

4

Go to the next page.

5

The Stop loading icon appears while the web server page is loading. Touch the icon to interrupt the load operation.

6

Reload the web server page. Touch Refresh icon and when the load operation starts, the icon changes to the Stop loading icon.

7

Go to the Start page. To configure the start page, refer to Start Page.

8

Touch the Menu icon to open Submenu A.

9

Touch the Change server icon to open Submenu B, where you can select the web server to display.

10

Touch the Zoom icon to open Submenu C, where you can adjust the zoom level from 25 to 500%. The default setting is [100%]. Touch the Reset icon (D) to return the magnification to its default value.

11

Touch the Settings icon to display the System Settings. For more information, refer to System Settings Menu.

12

Displays the selected web server page.

To scroll in the desired direction on the browser screen, slide your finger across the touch panel. To zoom in or out, pinch in or out on any area of the screen.

13

Touch the screen to display these scroll buttons.

If you want to hide these arrows, change the settings in System Settings > Browser. For more information, refer to Browser.

When the server uses a self-signed certificate, the message dialog "Server's certificate not trusted" appears upon the initial connection. Touching OK button will prevent this message from appearing again.

Software Keyboard

If the software keyboard is enabled, a virtual keyboard will pop up when you touch an input area on the browser.

You can switch keyboard types by touching the gear icon.

The SHOW/HIDE key toggles between showing and hiding the character input display area.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?