EIO0000005724.00

Precautions for Building into an End-use Product

This product is designed for use on flat surfaces of IP66F, IP67F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12 or Type 13 enclosure.

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is not designed for outdoor use. UL certification obtained is for indoor use only.

  • Install and operate this product with its front panel facing outward.

NOTE: IP66F and IP67F are not part of UL certification.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?