Factory Reset
You can restore this product to the state it was in at the time of purchase. Only an administrator account can perform this function.
To perform a factory reset, rebooting the product is required.
After rebooting, the steps for factory reset differ depending on whether you are using a password or not.
When using password
For instructions, refer to Factory Reset (When password is used).
When NOT using password
To perform a factory reset, create a reset key file and save it to external storage.
For instructions, refer to Factory Reset (When password is not used).
|
Function |
Description |
|---|---|
| Save to USB storage |
Create a reset key file and save it to the root of the USB storage device. |
| Eject USB storage |
Disconnect (unmount) the USB storage. Confirm the USB storage LED is off, then remove the USB storage device from the product. |
| Execute |
Use the reset key file in the SD card to perform a factory reset. |
| Eject SD card |
Disconnect (unmount) the SD card. Confirm the SD card access LED is off, then remove the SD card from the product. |