EIO0000005724.00

Change Password

This section describes how to change the password when it is being used for authentication.

NOTE: If you are not using a password and want to change to using a password, reset the password settings. Refer to Reset Password.
  1. Login to System Settings.
    NOTE: For instructions on how to access System Settings, refer to How to Display the System Settings.
  2. From the menu, select Security > Password.
  3. Enter the current password for the logged in user.
  4. Enter the new password and touch the Register button.
    NOTE:
    • Passwords should be at least 8 characters long and include at least one uppercase letter, one lowercase letter, one number, and one special character.

    • If you don't want to use password authentication, select Do not use password. If you created another user account in addition to the administrator account, delete that user account first. You can delete the user account by selecting Security > User Account from the menu.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?