EIO0000005724.00

Adding/Deleting a User Account

Create a standard user account separate from the administrator account created during setup. Only the administrator can add and delete user accounts.

NOTE:
  • Only one standard user account can be added.

  • If the administrator account is set to not use a password, you will not be able to create a standard user account.

  • To protect your product from unintentional changes to the configuration, we recommend that you use the standard user account for normal product operations.

  1. Login to System Settings.
    NOTE: For instructions on how to access System Settings, refer to How to Display the System Settings.
  2. From the menu, select Security > User Account.
  3. Enter the username and password, then touch Register button.
    NOTE:
    • Your password must be at least eight characters long and contain at least one uppercase letter, one lowercase letter, one number, and one special character.

    • If you forget the password, delete the standard user account and create a new one. Please note that if you perform the password reset function, the administrator account will also be deleted.

    • If you don't want to use password authentication, select Do not use password. In this case, the standard user account is used by default and the login screen will not display.

Delete user account

From the menu, select Security > User Account.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?