EIO0000005724.00

Precaution When Handling the SD Card

NOTICE
LOSS OF DATA
When using a SD card:
  • Make sure you regularly back up the SD card data.
  • While a SD card is accessed, do not turn off or reset this product, and do not remove the SD card.
  • Before removing the SD card from this product, stop all operations on the SD card.
  • Make sure of the SD card's orientation before inserting it into the SD card slot.
Failure to follow these instructions can result in equipment damage.
NOTICE
LOSS OF DATA
When handling the SD card:
  • Avoid storing the SD card where there is static electricity or electromagnetic waves.
  • Avoid storing the SD card in direct sunlight, near a heater, or other locations where high temperatures can occur.
  • Do not bend the SD card.
  • Do not drop or strike the SD card against another object.
  • Keep the SD card dry.
  • Do not touch the SD card connectors.
  • Do not disassemble or modify the SD card.
  • Use only SD cards formatted with the specified file system.
Failure to follow these instructions can result in equipment damage.

The file systems that this product supports are FAT, FAT32, and exFAT. This product does not recognize external storage formatted with NTFS.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?