EIO0000005724.00

System Structure

This section describes the system configuration with this product and peripheral equipment.

NOTE:
  • The number of interfaces may vary depending on the model. Refer to Parts Identification and Functions.

  • External storage devices used with this product should be formatted with the FAT, FAT32, or exFAT file system.

*1 Refer to Accessories.

*2 A USB storage device, USB keyboard, USB mouse, and USB hub can be used. Multiple USB devices of the same type cannot be connected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?