EIO0000005724.00

Status LED (Front LED)

After the power is turned on, the normal status indication by the LED is: red light > blinking orange > green light.

Color Indicator HMI operation
Green ON In operation/Offline
Blinking (ON/OFF every 3 seconds) Backlight OFF*1
Orange Blinking Software starting up
Red ON Power is ON.
- OFF Power is OFF.

*1 Specify Backlight off in the System Settings. For information, refer to Power Saving.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?