EIO0000005724.00

Factory Reset (When password is not used)

To perform this function, both an optional SD card and a commercially available USB storage device are required. Please prepare external storage formatted with the FAT, FAT32, or exFAT file system.

  1. Display System Settings.
    NOTE: For instructions on how to access System Settings, refer to How to Display the System Settings.
  2. From the menu, select System > Factory Reset.
  3. Touch the Execute button. The product reboots.
  4. From the menu, select System > Factory Reset.
  5. Connect the USB storage to this product.
  6. Touch the Save to USB storage button. The reset key file is saved to the USB storage.
  7. Touch the Eject USB storage button. Then make sure the USB storage LED is off.
  8. Remove the USB storage from the product and connect it to a computer.
  9. Copy the key file from the USB storage and paste it into the root directory of the SD card.
  10. Remove the SD card from the computer and insert it into the product.
  11. Touch the Execute button. The factory reset is performed and the product reboots.
NOTICE
LOSS OF DATA
Do not turn off the power during initialization.
Failure to follow these instructions can result in equipment damage.
NOTE: The reset key file cannot be used to reset other products. Please perform a reset, product by product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?