EIO0000005724.00

Password

When using password

Change your password. For instructions, refer to Change Password.

NOTE: If no operations are performed on the screen for more than 10 minutes, you will be automatically logged out and returned to the login screen.

Function

Description

Use password/Do not use password

Select whether to require password authentication to access system settings.

NOTE:
  • If you change the setting from not using a password to using one, you will need to reset the password.

  • If a standard user account has been registered, it cannot be changed to Do not use password. Please delete the standard user account first, and then change the setting.

Enter Administrator Name/Enter User Name

The currently logged in username is displayed. If you want to change the name, enter one that is 4 to 100 characters long.

Current Password

Enter the password you are currently using.

New Password/Confirm Password

Enter the new password. Refer to Password Requirements.

Password Reset on Login Screen

If enabled, "Can't login" is displayed on the login screen. If you touch it, the password reset screen is displayed. For details, refer to Reset Password.

Default: Enable

NOTE: If disabled, you cannot reset the administrator password if you forget it. Please contact customer support. In this case, all data in the product will be lost.

Password Requirements

The password must meet the following requirements:

Number of characters

8 characters or more, 100 characters or less

Types of characters

Use at least one of each of the following types of characters:

  • Uppercase letter (A-Z)

  • Lowercase letter (a-z)

  • Number (0-9)

  • Symbol (special character):
    ! " # $ % & '(apostrophe) ( ) * + , - . / : ; < = > ? @ [ \ ] ^ _ `(grave accent) { | } ~

When NOT using password

If you want to change from not using password to using it, you need to reset your password. For instructions, refer to Reset Password.

To perform this function, both an optional SD card and a commercially available USB storage device are required. Please prepare external storage formatted with the FAT, FAT32, or exFAT file system.

NOTE: The reset key file cannot be used to reset other products. Please perform a reset, product by product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?