EIO0000005724.00

Interface

Function

Description

Touch Buzzer

Change the settings for the beep that sounds when operating the touch panel.

Default: Enable

Keyboard Type

When a USB keyboard is connected to the product, select the keyboard type from US (101), JP (106), or Azerty.

Default: US (101)

NOTE: The keyboard type setting takes effect after the product is restarted.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?