EIO0000005724.00

Part Numbers

Part Number List

Series

Display size

Part number

Harmony GTW6

10-inch wide

HMIGT6540WCDW

12-inch wide

HMIGT6640WCDW

15-inch wide

HMIGT6740WCDW

19-inch wide

HMIGT6840WCDW

NOTE: All part numbers may be followed by any letter or number.

Part Number Configuration

The following describes the configuration of model numbers.

Digit Category Number Description
1...3 (Prefix) HMI -
4...6 Series GT6 -
7 Display size 5 10"
6 12"
7 15"
8 19"
8, 9 Type 40 Advanced
10 LCD W Wide TFT
11 Touch panel C Multi (PCAP)
12 Power supply D DC
13 and later Supported software, others W Web HMI*1

*1 Not supported by screen editing software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?