EIO0000005724.00

Backup Restore

Back up data in the product to an external storage, and restore the product using the backup file in the external storage. Only an administrator account can perform this function.

To perform backup or restore, rebooting the product is required.

For instructions, refer to Recovery (Backup and Restore).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?