EIO0000005724.00

Factory Reset (When password is used)

  1. Login to System Settings.
    NOTE: For instructions on how to access System Settings, refer to How to Display the System Settings.
  2. From the menu, select System > Factory Reset.
  3. Touch the Execute button. The product reboots.
  4. Login to System Settings again.
  5. From the menu, select System > Factory Reset.
  6. Touch the Execute button. The factory reset is performed and the product reboots.
NOTICE
LOSS OF DATA
Do not turn off the power during initialization.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?