EIO0000005724.00

Precautions for Connecting the USB Cable

WARNING
EXPLOSION HAZARD
  • Verify the power, input, and output (I/O) wiring are in accordance with Class I, Division 2 wiring methods.
  • Do not use this product in hazardous environments or locations other than Class I, Division 2, Groups A, B, C, and D.
  • Substitution of any components may impair suitability for Class I, Division 2.
  • Do not disconnect equipment while the circuit is live or unless the area is known to be free of ignitable concentrations.
  • Remove power before attaching or detaching any connectors to or from this product.
  • Ensure that power, communication, and accessory connections do not place excessive stress on the ports. Consider the vibration in the environment when making this determination.
  • Securely attach power, communication, and external accessory cables to the panel or cabinet.
  • Use only commercially available USB cables.
  • Use only non-incendive USB configurations.
  • Suitable for use in Class I, Division 2, Groups A, B, C, D Hazardous Locations.
  • Confirm that the USB cable has been attached with the USB cable clamp before using the USB interface.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?