EIO0000005724.00

User Account

Add a user account. Only an administrator account can perform this function.

For instructions, refer to Adding/Deleting a User Account.

When you create the user account, a change account icon will appear at the top right of the screen. Touch that icon and the Change Account screen is displayed.

  1. Change account

NOTE: When you perform a password reset, all accounts are reset.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?