EIO0000005724.00

Product does not boot up properly

If for some reason the product does not boot up properly or you cannot open the System Settings, please try the following.

Within 15 seconds of turning on the product, or as soon as the boot screen (splash screen) disappears, double-tap the bottom-left or bottom-right corner of the screen. The product will open the System Settings.

If you prepared recovery media, use it to perform a restore.

Refer to Recovery (Backup and Restore).

If you have not performed a backup, perform a factory reset.

Refer to Initialization (Factory Reset).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?