EIO0000005724.00

Update the System

Updates the product system to the latest version. Keep the product system up to date to maximize product safety.

To perform this function, either an optional SD card or a commercially available USB storage device is required. Please prepare external storage formatted with the FAT, FAT32, or exFAT file system.

  1. Download the system update file for this product from our website.
    www.se.com/ww/en/download
  2. Unzip the downloaded file and save all files to the root folder of the external storage.
  3. Connect the external storage to the product and turn on the product.
  4. Display the System Settings. Refer to How to Display the System Settings.
  5. From the menu, select System > System Update. Then touch the Start button.
  6. The update process is started. Please wait a few minutes until the process is complete. The product will restart.
  7. Verify the system has been updated. Display the System Settings, then select Information from the menu.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?