EIO0000005724.00

Boot

Function

Description

Boot Image Mode

Change the default boot screen that displays at product startup. Select None to keep the default boot screen, or select Image to display a custom screen.

Default: Image

Boot Image Data

When Boot Image Mode is set to Image, touch the Load button to import an image file (file name: BootImg.png) from a USB storage device.

To the root folder of the USB storage device, save the file that meets the following conditions.

  • File size: Maximum 12 MB

  • File format: PNG

  • Image resolution: Maximum 2048 x 2048. Create an image with a resolution that matches the display resolution.

Delay Time

Set the delay time (0 to 300 seconds) between powering on the device and displaying the page specified in the Start Page field.

If the Delay Time is set to anything other than 0, after powering on, the screen will change as follows:

Boot image > Delay page > Start page

However, if you select System Settings as the start page, the System Settings screen will display immediately after the boot image, regardless of the Delay Time setting.

To set the start page, refer to Start Page.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?