Server
Register the web servers to connect. You can register up to 20 web servers located on the same intranet to this product.
|
Function |
Description |
|---|---|
| Server Name |
Set a server name of up to 32 characters to identify the server. The name you set here will appear in the Start Page settings and when selecting a server in the browser. Only alphanumeric characters (uppercase, lowercase, and numbers) are allowed. |
| Server URL |
Set the IP address of the web server in URL format. Set a URL of up to 256 characters, including alphanumeric characters and special symbols. NOTE: Always include "http://" or "https://" as a prefix before the IP Address (or hostname).
Example: If
the web page is on a specific port (port: 8080). |
| Software Keyboard |
Set whether to display software keyboard in the browser. Default: Enable |
| Server Connectivity |
Touch the Test button to check the connection status with the web server. |