EIO0000005724.00

System Settings Menu

This section describes the functions provided in the System Settings.

 

Function

Description

A

Switching accounts

Switch user accounts.

This function is displayed if you have a standard user account in addition to the administrator account.

B

Reboot

Reboot the product.

Menu

Description

Information -

Displays the system status, version information, etc.

System System Monitor

Displays the number of times this product has been started, the total operating time, the temperature inside the product, etc. This also exports the system settings operation log.

Date and Time

Set the product's internal clock.

Language

Select the user interface language for the system settings.

Interface

Configure the buzzer sound for touch operations and the settings for using external USB keyboards.

Power Saving

Configure the product's behavior when it is not in use.

System Update

Update the firmware and operating system of the product.

Factory Reset*1

Resets the product to the state it was in when it was purchased.

Backup Restore*1

Back up the data in the product to a USB storage device and use the backup file to restore the product.

Display Display1

Configure display settings such as brightness and touch areas.

Ethernet*1 ETH1/ETH2

Configure the Ethernet settings.

Boot -

Change the default boot screen displayed at product startup.

Browser -

Configure the display settings for the browser.

Server Start Page

Select the initial screen displayed after the product starts up.

Server

Register the web servers to connect.

Security*2 Password

Change the login password.

User Account*1

Register or delete standard user accounts separate from the account with administrator privileges.

Firewall*1

Configure settings related to the firewall.

External Access*1

Set whether to allow remote access to system settings.

*1 Displays only if you are logged in with an administrator account.

*2 If password authentication is not used, this setting is not displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?