EIO0000005724.00

Touch Panel

Touch panel type Projected capacitive (PCAP) with optimized noise filter
Touch points Multi-touch (two-point touch)
Touch panel service life 50 million times or more
Touch panel resolution 2,048 x 2,048
Touch mode Standard mode, Water detection mode, Glove mode
NOTE: Change the mode in the System Settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?