EIO0000005724.00

System Monitor

Displays the number of times this product has been started, the total operating time, the temperature inside the product, etc.

Function

Description

System Statistic

Displays the number of times this product has been started, the total operating time, the temperature inside the product, etc.

Boot times and Accumulated operation time are not cleared even though you perform a factory reset or restore.

Free Memory

Set to automatically restart the product when the remaining memory falls below the specified percentage. Restarting the product clears the temporary data and frees up memory.

Default: 0 (Disable)

Export System Log

Exports the system settings operation log to external storage.

To remove external storage after exporting the log data, touch the Eject storage device button. Make sure the corresponding LED is off, and then remove the external storage from the product.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?