EIO0000005724.00

Power Saving

Function

Description

Mode

Set up the screen saver status for when the time defined in the Timer field elapses. Selecting Backlight off, turns off the backlight.

Default: None

Timer

Set the duration (1 to 300 minutes) of inactivity (no touch operations) before the screen saver starts.

Default: 0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?