EIO0000005724.00

Product Overview

This product is an industrial display equipped with a dedicated HTML5-compatible browser. As a Web client, the product can access Web servers on the same Intranet and display the server content in the dedicated browser.

  • The dedicated browsers support CSS3 and XML.

  • You can connect to HTML5 servers (such as an HMI, IPC, PLC, or other external device with Web server functionality) that support JavaScript or HTTPS. You can connect to up to 20 web server devices. The recommended browser is Google Chrome.

  • You cannot use this product on the Internet.

  • HMI applications do not run on this product.

After turning on this product, you need to set up its display and Web browser settings. For information about settings, refer to Setup.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?