EIO0000005724.00

Display On Device

On the product screen, switch to the system settings screen from the web server page.

  1. From the top part of the screen, slowly swipe downward with force. The title bar of the browser appears.
  2. Touch the Menu icon located on the right side of the title bar. This will open a submenu. From the submenu, select the Settings icon.
  3. The System Settings display. If "Use password" is set, the login screen displays. Enter your username and password to log in.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?