EIO0000005724.00

Maintenance Accessories

This section lists replacement parts.

Product name

Product number

Description

Installation Fastener

Installation Fastener

HMIZCAF1

Fastener for installing the product into a solid panel (4 pieces/set).

Installation Gasket

Installation Gasket for 10-inch wide

HMIZD55W

Provides dust and moisture resistance when 10-inch wide model is installed into a solid panel (1 piece).

Installation Gasket for 12-inch wide

HMIZD56W

Provides dust and moisture resistance when 12-inch wide model is installed into a solid panel (1 piece).

Installation Gasket for 15-inch wide

HMIZD57W

Provides dust and moisture resistance when 15-inch wide model is installed into a solid panel (1 piece).

Installation Gasket for 19-inch wide

HMIZCWG8W1

Provides dust and moisture resistance when 19-inch wide model is installed into a solid panel (1 piece).

Power Supply Connector

Power Connector (DC)

HMIZCCNDC1

Connector with fixable screws to connect DC power supply cables (Straight type, 5 pieces/set).

USB Cable Clamp

USB Clamp Type-A (1 port)

HMIZGCLP1

Clamp to prevent disconnection of USB cable (USB Type-A, 1 port, 5 clamps/set).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?