EIO0000005724.00

Date and Time

Set the clock on the product.

Function

Description

Date/Time

When the NTP server is disabled, set the date and time on the product.

Timezone

Select the time zone (region) in which the product is used.

Synchronized with NTP Server

Select whether to adjust the time so that it is synchronized with an NTP server.

Default: Disable

NTP Server

Set the NTP server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?