About the Document
Document Scope
This document describes the specifications, installation, operation, and maintenance of the Harmony GTW6, which is a Web HMI (Human Machine Interface) device used in industrial or factory automation systems.
This document is intended for users who design systems, or install and maintain components.
Validity Note
This document is valid for the Harmony GTW6.
The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.
Product Related Information
This product has been designed, developed and manufactured for use in industrial or factory automation systems.
-
The product is not appropriate for use with aircraft control devices, medical life-support equipment, central trunk data transmission (communication) devices, or nuclear power control devices, due to inherent requirements for extremely high levels of safety and reliability.
-
When using the product with transportation vehicles (trains, cars, and ships), disaster and crime prevention devices, safety equipment, or medical devices unrelated to life-support systems, use redundant and/or failsafe system designs to ensure reliability and safety.
If the equipment is used in a manner not specified by the manufacturer, the protection provided by the equipment may be impaired.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Critical alarm indicators and system functions require independent and redundant protection hardware and/or mechanical interlocks.
Please design a safety circuit external to this product so that the entire system operates safely even if the external power supply or this product fails or malfunctions.
-
Interlocks and other circuits designed to interrupt or prevent equipment operation (such as emergency stops, protective circuits, and opposing action circuits) and circuits that prevent machine damage, such as positioning mechanisms, should be constructed external to the product.
-
The product stops operation when it detects an abnormality such as a watchdog timer error. If an error occurs in the input/output control area, which cannot be monitored, it may lead to unexpected input/output behavior. Therefore, it is important to configure an external fail-safe circuit or mechanism.
-
Problems with the relay or transistor in the output unit may cause the output to remain either in the ON or OFF state. Install an external monitoring circuit for output signals that may cause a serious accident.
Design the circuit so that power is supplied to the external device or load control power supply connected to this product before it starts.
When you cycle power, wait at least 10 seconds after it has been turned off. If this product is restarted too quickly, it may not operate correctly.
Do not create any switches on the touch panel that may cause personal injury, property damage, or compromise the safety of the equipment. Design the system so that controls for important operations are managed by devices other than this product, or by independent hardware switches.
In the event the screen cannot be properly read, for example, if the backlight is not functioning, it may be difficult or impossible to identify a function. Functions that may present a hazard if not immediately executed, such as a fuel shut-off, must be provided independently of this product.
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control" and to NEMA ICS 7.1 (latest edition), "Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems" or their equivalent governing your particular location.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
When communication with the server is lost, the behavior of this product during operation depends on the server-side screen design. For example, if a momentary switch is being touched when communication is interrupted, the server may interpret it as the end of the touch operation. The screen should be designed so that the system behaves safely, even if communication is lost in the middle of an operation.
The following characteristics are specific to the LCD panel and are considered normal behavior:
-
LCD screen may show unevenness in the brightness of certain images or may appear different when seen from outside the specified viewing angle. Extended shadows, or crosstalk may also appear on the sides of screen images.
-
LCD screen pixels may contain black and white colored spots and color display may seem to have changed.
-
When experiencing vibrations within a certain frequency range and vibration acceleration is above what is acceptable, the LCD screen may partially turn white. Once the vibration condition ends, the whitening of the screen is resolved.
-
When the same image is displayed on the screen for a long period, an afterimage may appear when the image is changed.
-
The panel brightness may decrease when used for a long time in an environment continuously filled with inert gas. To prevent deterioration of panel brightness, regularly ventilate the panel. For more information, please contact customer support.
www.se.com/support
WARNING |
|---|
|
SERIOUS EYE AND SKIN INJURY
The liquid in the LCD panel contains an irritant:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
REDUCED SERVICE LIFE
Change the screen image periodically and try not to display
the same image for a long period of time.
Failure to follow these instructions can result in equipment damage.
|
Precautions on using models with projected capacitive touch panel
Models with a projected capacitive (PCAP) touch panel may operate abnormally when the display surface is wet.
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
-
When Touch Mode is set to Water detection mode, an abnormal touch (such as accidental contact with water or other liquids) will temporarily disable touch for a few seconds to avoid unintended operations. Normal touch operation recovers a few seconds after the abnormal touch condition is removed. You can change the Touch Mode in System Settings.
-
While the system is starting up, as the touch panel initial values are being checked, do not touch the touch panel area.
| NOTICE |
|---|
|
EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
Compared to conventional analog resistive film, projected capacitive touch panels have higher transmittance and lighter touch operation, as well as supporting multi-touch. As it is able to detect weak changes in capacitance, projected capacitive touch panels are susceptible to environmental noise.
While our products have been optimized for industrial environmental noise and conform to CE marking, our products cannot support all environmental noise.
Please consider the following in the installation environment to avoid touch malfunction.
Example:
To reduce the noise voltage of the enclosure of the equipment housing this product:
-
Implement noise countermeasures in the equipment. For example, install a noise filter on the inverter, servo amplifier, or other equipment. Refer to the manufacturer's instruction manual.
-
Attach a ground wire noise filter to the FG connection of equipment.
-
Connect the enclosure for the equipment to the building. For example, connect to the concrete or steel reinforcement parts of the building.
General Cybersecurity Information
In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.
To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.
Schneider Electric provides additional information and assistance:
-
Subscribe to the Schneider Electric security newsletter.
-
Visit the Cybersecurity Support Portal web page to:
-
Find Security Notifications.
-
Report vulnerabilities and incidents.
-
-
Visit the Schneider Electric Cybersecurity and Data Protection Posture web page to:
-
Access the cybersecurity posture.
-
Learn more about cybersecurity in the cybersecurity academy.
-
Explore the cybersecurity services from Schneider Electric.
-
Product Related Cybersecurity Information
Refer to Cybersecurity.
Environmental Data
For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.
Available Languages of the Document
The document is available in these languages:
Related Documents
|
Title of documentation |
Reference number |
|---|---|
|
Cybersecurity Best Practices |
Refer to General Cybersecurity Information. |
|
HMI/IPC Cybersecurity Guide |
You can download the manuals related to this product, such as the software manual, from the Schneider Electric download center (www.se.com/ww/en/download).
Information on Non-Inclusive or Insensitive Terminology
As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.
Trademarks
Microsoft® and Windows® are registered trademarks of Microsoft Corporation in the United States and/or other countries.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.
Google Chrome is a trademark of Google LLC.
Product names used in this manual may be the registered trademarks owned by the respective proprietors.
DANGER
WARNING