EIO0000005724.00

Setup

After turning on the product for the first time, perform the system setup.

In the System Settings, configure the product's hardware configuration and network settings such as IP addresses.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?