EIO0000005724.00

Removing the SD Card

If you remove the SD card while it is in use, you risk corrupting the data. Before removing the SD card from this product, stop all operations on the SD card.

  1. Make sure the SD card access LED is off, then open the SD card slot cover. To open the slot cover, lightly push the edge of the cover in the direction of the arrow.

    A. SD card slot cover

  2. Push the SD card once to release, then pull out the card.
    NOTE: After using the SD card, store the SD card in its case or in another safe location.
  3. Close the SD card slot cover.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?