Parts Identification
|
A. Status LED (front LED) |
K. Expansion unit interface (unavailable)*2 |
|
B. Battery slot |
L. Status LED (STA) |
|
C. SD card slot cover |
M. Error LED (ERR) |
|
D. Serial interface (COM2) (unavailable) |
N. COM1 LED (COM1) |
|
E. Serial interface (COM1) (unavailable) |
O. COM2 LED (COM2) |
|
F. Ethernet interface (ETH2)*1 |
P. USB storage LED (USB) |
|
G. Ethernet interface (ETH1) |
Q. SD card access LED (SD) |
|
H. USB (Type-A) interface (x 2) |
R. Safety alert symbol*3 |
|
I. USB (micro-B) interface (unavailable) |
S. Safety alert symbol*4 |
|
J. Power connector |
*1 The factory default for the ETH2 port is disabled. Use the System Settings to change it. For details, refer to Ethernet.
*2 Do not remove the sticker attached to the rear of the product.
*3 Identifies the safety messages about the battery in Replacing the Battery.
*4 Identifies the safety messages about the USB (micro-B) interface in Cable Connections.