EIO0000005724.00

Display

Configure display settings such as brightness and touch areas.

Function

Description

Brightness

Set the display brightness.

Optimize the capacitance

Optimizing for capacitive touch. Wipe the screen clean to begin. Do not touch the screen until the process is complete.

NOTE: This setting is visible on the device screen only. It does not appear when you access the System Settings remotely from a personal computer.
Orientation

Select either Landscape or Portrait for the product's installation orientation.

Default: Landscape

Touch Check

Check the operation of the touch panel. The touched position will be highlighted.

NOTE: This setting is only visible on the device's screen. It doesn't appear when you access the System Settings remotely from a personal computer.
Touch Mode

The following three modes are available to support your usage environment. Select the mode according to your usage environment.

Standard Mode: Suitable for touch operations using your finger.

Water Detection Mode: Mode where touch input becomes disabled when there are liquids, such as drops of water, on the screen. Suitable to prevent touch panel mis-operation due to liquids on the screen. After wiping the liquid or other foreign substance from the screen, touch input becomes enabled in about 2 seconds.

Glove Mode: Mode suitable for use with gloves, such as rubber gloves.

Default: Standard Mode

NOTE:
  • Depending on the type of glove, operation may not be possible.

  • Because touch sensitivity is increased in this mode, it is more susceptible to environmental noise.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?