EIO0000005724.00

Set Up On Device

This section describes how to configure the product on screen.
  1. Power on the product.
  2. The Create Account screen is displayed. Create an administrator user account for the System Settings. Enter the username and password, then touch the Register button.
    NOTE:
    • Passwords should be at least 8 characters long and include at least one uppercase letter, one lowercase letter, one number, and one special character.

    • Although you can operate the product without using password authentication, we recommend setting a password to keep the product secure.

    • The Skip button does not work on this model.

    • You can change the password at any time. For details, refer to Change Password.

  3. The Login screen is displayed. Enter the username and the password set earlier, then touch the Login button.
  4. The System Settings menu screen is displayed. Select System > Date and Time to set the clock, and then touch the Save button.
  5. From the menu, select Ethernet. Change the network settings as required and touch the Save button.
  6. From the menu, select Server > Server to register Web server devices that are connected to the same Intranet. From the menu's Start Page option, you can specify the Web server that displays first after the product starts.
  7. From the menu, select Browser and adjust the settings to match the conditions of the target web server.
  8. Change other settings as required. For information on system settings functions, refer to System Settings Menu.
    NOTE: When creating the administrator account, if you selected the Use password option, you can add other user accounts. For information, refer to Adding/Deleting a User Account. Use the account that matches the specified use, such as using a standard user account for normal operations, and using the administrator account only for system development and maintenance.
  9. Touch the reboot icon at the top right of the screen. The product will restart and display the screen set as the Start Page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?