BQT6904800 -04

Access to the MCSeT Cubicle Compartments

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Make sure that the truck is in disconnected/test position before opening the front door.
  • Turn off all power supply or de-energize the complete cubicle because opening any door is not allowed if the busbar or cable is live.
Failure to follow these instructions will result in death or serious injury.

Figure 53
Access to the Main Circuit Compartments of I/F Cubicle

1

Access to the LV compartment

4

Front access to the cable compartment

2

Front access to the busbar compartment

5

Rear access to the cable compartment

3

Access to the VCB compartment

6

Rear access to the busbar compartment

NOTE: The image shown here are for illustration purpose only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?