BQT6904800 -04

Operating the VCB

VCB Controls and Indicators

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR BURN
  • Installation, repair, and maintenance work on the EvoPacT HVX VCB must only be carried out by qualified and certified personnel.
  • Beware of potential danger, apply appropriate PPE.
  • Follow safe electrical work practices.
Failure to follow these instructions will result in death or serious injury.

Table 15 Position Indicator

Item

Energy-storing device (spring mechanism)

VCB ON/OFF

Possible operating sequence

1

Released

OFF

None

2

Charged

OFF

C–O

3

Released

ON

O

4

Charged

ON

O–C–O

C = Switching ON (Closing)

O = Switching OFF (Opening)

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.