DOCA0006EN-08

Date/time format

The date is displayed in the following format: DD-MMM-YYYY.

The time is displayed using the 24-hour clock in the following format: hh:mm:ss.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.