DOCA0006EN-08

About this manual

Document scope

This manual is intended for use by designers, system builders and maintenance technicians with an understanding of electrical distribution systems and monitoring devices.

Throughout the manual, the term “meter” / device” / “equipment” / “product”refers to all models of the PM3200 series. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.

This manual does not provide configuration information for advanced features where an expert user would perform advanced configuration. It also does not include instructions on how to incorporate meter data or perform meter configuration using energy management systems or software, other than ION Setup.

Related documents

Document

Number

PM3200 / PM3210 instruction sheet

S1B46605 / S1B62913

PM3250 / PM3255 instruction sheet

S1B46607 / S1B62914

You can download these technical publications and other technical information from www.se.com.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.