DOCA0006EN-08

Modifying a numerical value

When you modify a numerical value, the digit on the far right side is selected by default (except for Date/Time). The following parameters are the only ones for which you set a numerical value:

  • Date

  • Time

  • VT primary

  • CT primary

  • Password

  • Modbus address of the meter

  • Pickup setpoint

  • Dropout setpoint

  • Time delay / Interval duration

To modify a numerical value:

  1. Use the or button to modify the selected digit.
  2. Press to confirm the new parameter value and to shift to the next digit. Modify the next digit, if needed, or press .
  3. Continue to move through the digits until you reach the last digit then press again to confirm the new parameter value.
    NOTE: If you enter an invalid setting and press cursor stays in the field for that parameter until you enter a valid value.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.