DOCA0006EN-08

Power quality analysis values

The power quality analysis values use the following abbreviations:

  • HC (Harmonic Content) =

  • H1 = Fundamental Content

  • THD (Total Harmonic Distortion) = HC/H1 X 100%

THD provides a measure of the total distortion present in a waveform. THD is the ratio of harmonic content to the fundamental and provides a general indication of the quality of a waveform. THD is calculated for both voltage and current.

The following table lists the power quality values of the meter:

Power quality values (PM3210 / PM3250 / PM3255)

Characteristics

Description

THD

Per phase current and per phase voltage (L-L and L-N) Most distorted of 3 phases

Average of 3 phases *

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.